Part Number: DCA1000EVM
I have a AWR1642EVM ES:1 and DCA1000EVM. The mmwaveStudio I used is 1.0. But when I click "setupDCA1000" button in mmwaveStudio and click "connect reset and" button, the FPFA Version is still 0.0.0.0 and the output window shows "Ethernet Cable is disconnected Please check.....!!!". I think i connected everything correctly and switchs in the DCA1000EVM are put on the right position.I have tried reflashing the DCA1000EVM but it still show the same error. So what can i do?