Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR1642, AWR1642
I need to be able to have the sensor reboot itself if there is no serial port activity. Is there a sample or an api call to to reboot. On the 2640 I called SysCtrlSystemReset(); Which directly wrote to registers. Is there an equivalent function for the IWR1642?
Also, is there a way to initiate a reboot via the usb port. Is there some command that i can issue via serial port to reset the unit via XDS110. In the documentation, it states that the XDS110 uses SW2 (a hardware switch) to reset the unit. How can i externally make this happen via USB.