This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMP91300: measurements on two same PCB's differ from each other

Expert 6470 points
Part Number: LMP91300
Other Parts Discussed in Thread: LDC1101, LDC1614

Team,

we've made a design of the PNP sensor with the LMP91300. I measured two PCBs with LMP91300 on each of them (D4 and D5), the device/PCB D4 shows totally different measurement values than the device D5.

The one measurement is average value from 22 values of the proximity register. I changed between those PCBs the capacitor CF (CF_4 <-> CF_5), CBY (CBY_4 <-> CBY5), thermistors, coils (the coils inductance is approximately 165uH). It's still the same.

Can you help to understand why is there such a big difference between D4 and D5? Where are we making a mistake?

Schematic, layout, register values and measurement values we can share offline.

Thank you for your prompt help.