Part Number: IWR6843ISK
Other Parts Discussed in Thread: IWR6843, MMWAVEICBOOST, UNIFLASH,
Hi,
I am a new user of TI's IWR6843 mmWave sensor kit. I have a whole setup of IWR6843 + mmWAVEICBooster + DCA1000 data acquisition module setup connected to a 5 V source. The current consumed by this setup is close to 880 mA. The mmWAVEICBooster kit is connected to my Windows 7 laptop through the XDS110 microUSB port. I see there are two COM ports on my Device Manager list - XDS110 Class Application/User UART (CFG_port) and XDS110 Class Auxilliary Data Port (Data_port).
My problem now is that, the mmWave Demo Visualizer web app is not able to recognize the board. I keep getting the "Hardware Not connected" message again and again. I opened the COM ports using Putty to verify my results. I came across this post on the Forum and as it says, is there an issue with the FTDI/XDS Drivers on Windows? Please, do let me know. I have attached the photo of the mmWAVEICBoost and my setup.
Thanks,
Vijay