Part Number: IWR6843
Hi
We're using the IWR6843 for our project.
In our application we need to regulate the TX transmitting power of the IWR6843 in oder to make sure that the transmitting power stays always the same over different temperature and aging.
Therefore could you help us with the following information:
- Is the IWR6843 TX transmitting power configurable?
- Is there an integrated power detector in the IWR6843?
- If not, do you have any suggestion: how can we regulate the IWR6843 transmitting power? since it's very important for us to make sure the transmitting power stays relative constant over all conditioning.
Thanks very much
Bien