This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: Is hardware trigger supported?

Part Number: IWR6843

According to the user guide in the SDK (at least 03_02_00_04 and 03_03_00_03) the hardware trigger is not supported.

From page 22 (SDK 03_03_00_03):

I have confirmed that it works, I get frames when I put the pin high and none when low, but there is no sense in relying on it if it is not supported (and risk being removed or can cause problems).