This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-RF-EVM: Radar object detect use case clipping maximum range at around 15 meters irrespective of settings.

Part Number: MMWCAS-RF-EVM


Hi, 
I'm evaluating Radar SDK use case on MMWCAS-RF-EVM mounted on MMWCAS-DSP-EVM, specifically the use case radar_object_detect. 

cascade_radar_object_detect.zip

These are my CC, coefficient.bin, coefficient script, and the use case demo script files. I have changed almost every parameter inside the Matlab script but for some reason the RADAR clips the maximum range to 15 meters. I tried all of the profile numbers as well as the modes supported by the demo script but nothing changed the maximum range of 15m. 

The other peculiar thing is each of the graphs has a different maximum range. For instance, during one of my evaluation runs, the range doppler profile shows a maximum distance of 2000 meters whereas the RDM and Range doppler points only show a maximum of 150 meters(as shown below). In the range doppler profile it shows that I covered 2000m but in reality, I only go up to 15. Changing the sampling frequency or the frequency slope didn't help either. 

I suspect there's a very basic setting that I'm overlooking that unlocks the full range of MIMO but I cannot locate it at this moment. All help is appreciated.