Other Parts Discussed in Thread: IWR6843
I'm trying to use DCA1000EVM with MMWAVEICBOOST on mmWave Studio 2.1.0.0. I have installed all the relevant software in mmWave Studio user guide, and DCA1000EVM user guide. My computer is connected to both of the devices, with static IP configured as given, and firewall disabled.
When I’m triggering a frame (following instruction like in the https://training.ti.com/dca1000-training-video
I get a Timeout Error! System disconnected (see log1 below)
when I'm trying to use DataCaptureDemo_xWR.lua, modified the script by adding a delay
RSTD.Sleep(2000) after ar1.CaptureCardConfig_StartRecord(adc_data_path, 1) (as recommended in another thread )
I receive "no of files captured is zero error". (cf log 2 below)
log1:
15:59:14] [RadarAPI]: Sending fpga_version command to DCA1000
[15:59:14] [RadarAPI]:
[15:59:14]
[15:59:14] FPGA Version : 2.7 [Record]
[15:59:14]
[15:59:26] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[15:59:26] [RadarAPI]: Sending start_record command to DCA1000
[15:59:47] [RadarAPI]: ar1.StartFrame()
[15:59:47] [RadarAPI]: Status: Passed
[15:59:47] Frame start async event received!
[15:59:47] [RadarAPI]: Frame Ended
[16:00:46] [RadarAPI]:
[16:00:46] Start Record command : Success
[16:00:46]
[16:00:46] Record Process :
[16:00:46] Timeout Error! System disconnected
[16:00:46]
[16:00:46] Record stop is done successfully
[16:00:46] Frame End async event received!
[16:00:46] [RadarAPI]:
log2:
[16:02:53] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 0)
[16:02:54] [RadarAPI]: Sending fpga command to DCA1000
[16:02:54] [RadarAPI]:
[16:02:54] FPGA Configuration command : Success
[16:02:54] CaptureCardConfig_Mode Success
[16:02:54] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
[16:02:54] [RadarAPI]: Sending fpga command to DCA1000
[16:02:54] [RadarAPI]:
[16:02:54] FPGA Configuration command : Success
[16:02:54] [RadarAPI]: Sending record command to DCA1000
[16:02:54] [RadarAPI]:
[16:02:54] Configure Record command : Success
[16:02:54] CaptureCardConfig_PacketDelay Success
[16:02:54] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin", 1)
[16:02:54] [RadarAPI]: Sending start_record command to DCA1000
[16:02:54] [RadarAPI]: Status: Passed
[16:02:57] [RadarAPI]: ar1.StartFrame()
[16:02:57] [RadarAPI]: Status: Passed
[16:02:57] Frame start async event received!
[16:02:57] [RadarAPI]: Frame Ended
[16:02:57] Frame End async event received!
[16:03:02] Please wait for a few seconds for matlab post processing .....!!!!
[16:03:02] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin")
[16:03:02] [RadarAPI]: , Total no of frames for each device : 8
[16:03:02] Error : The number of files captured is zero!
[16:03:12]
[16:03:12] ***Script completed successfully.***
Thanks for your help