Part Number: TDA4VM
In TDA4VM TRM, it is declared that DISPC supports YUV422 output pixel format. But only BT.656/BT.1120 are specified.
We need BT.601 output over a 12-bit hardware interface. Can it be supported?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VM
In TDA4VM TRM, it is declared that DISPC supports YUV422 output pixel format. But only BT.656/BT.1120 are specified.
We need BT.601 output over a 12-bit hardware interface. Can it be supported?
Hi Alex,
for BT.601 support please check the following sections of the DRA829/TDA4VM/AM752x Technical Reference Manual (Rev. A):
12.6.2.1 DISPC Environment
12.6.2.1.4 VSYNC/HSYNC/DE Signal Export to SoC Boundary
Regards,
Yordan
Hi Yordan,
Thanks for the information.
It seems that BT.601 can be supported with alternative VP1 output.
But here comes a question about the data pins.
As described in section 12.6.2.1.2, the bits [9-2] are effectively used in BT.656 mode (should be the same for BT.601).
The two LSBs are ignored. Then what HW pins should we connected to the external BT.601 display device (actually it's a serializer)?
Keep data[9-0] or just data[9-2]?
Hi Alex,
If you require 8bit output, then use D[9:2] lines.
Rgds,
Brijesh
Hi Alex,
I have information from TRM team regarding your question:
data[9-2] pins should be connected. At DSS side, data[1-0] are always ‘0’ when BT.656 mode is selected.
Regards,
Yordan