Part Number: IWR6843
Dear TechnicalSupport
I use IWR6843 ISK(ES2.0) following FW was burned.
C:\ti\mmwave_industrial_toolbox_4_2_1\labs\people_counting\68xx_3D_people_counting\prebuilt_binaries\3D_people_count_68xx_demo.bin
I walked a distance of 15m from right below in the y-axis direction.
The result is that the point cloud looks above the person's head.
Is there any correction applied to the z-axis direction?

But, In the user guide, the supported device is written as ISK.
Is it correct that I can use it for both ODS and ISK?
C:\ti\mmwave_industrial_toolbox_4_2_1\labs\long_range_people_detection\68xx_long_range_people_det\prebuilt_binaries\long_range_people_det_68xx_demo.bin
Best Regards