Other Parts Discussed in Thread: AWR1642
Hi,
This is an extension of the previous relevant question. Please refer URL for reference : e2e.ti.com/.../894294
I am learning TI mmwave sensors using AWR1642BOOST (ES2.0) + DCA1000 EVM with a Windows 10 laptop and mmwave Studio 02.00.00.02. I am collecting 2x complex data from the ADC.
(Please note that I cannot upgrade to mmwave Studio 2.1.0.0 )
1) As guided in the above question, I referred "numAdcSamples" variable at location file:///C:/ti/mmwave_sdk_03_03_00_03/packages/ti/control/mmwavelink/docs/doxygen/html/structrl_profile_cfg__t.html
It states that : Valid range: 2 to MAX_NUM_SAMPLES
However, in mmwave Studio tab " SensorConfig" , I found that I cannot set number of ADC samples less than 64. Please advise how can I set the number of ADC samples less than 64 in mmwave Studio 2.0.0.2. I particular, I wish to set the number of ADC samples to 8 or 4.
2) I wish to set the start the Tx frequency as 77 GHz and I wish to experiment with very short bandwidth, say 90 MHz or even less. Please advise how can I set this bandwidth in mmwave Studio 2.0.0.2 ? Should I set it in tab " StaticConfig " of mmwave Studio 2.0.0.2 ? Or is there some other way to set the bandwidth of Tx signal ?
Please also advise that is there any lower limit of bandwidth that could be set for Tx signal ? If yes, then please advise TI document(s) stating that limit for the AWR1642 device, for TI Demo Visualizer and for mmwave Studio 2.0.0.2.
Thanks and regards