Part Number: DCA1000EVM
Other Parts Discussed in Thread: IWR1843, IWR1843BOOST, AWR1843BOOST
Hello officers,
"MSS Power Up async event was not received!" problem happened in SPI connecting stage. I have searched this problem on forum, and I have already given the erase command to board through Uniflash, but it still dosen't work. I also checked SOP to mode 2 and put switch 2 to SPI mode. Beside, I have checked that 6 ports are listed in device manager properly.
I use mmWave Studio 2.1.0.0
There is my output:
GM: Constructor
GM: Sat Jan 23 12:21:18 2021
RSTD.Transmit("/Settings")
[12:21:18]
[12:21:18] ### Running Startup script: "C:\ti\mmwave_studio_02_01_00_00\mmWaveStudio\Scripts\Startup.lua" ###
[12:21:18] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[12:21:18] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[12:21:18] Scripter ignored: Attempt to UnBuild() again or before Build.
[12:21:18] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\Clients\\\\LabClient.dll")
[12:21:18] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[12:21:18] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[12:21:18] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[12:21:18] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[12:21:18] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[12:21:18] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_02_01_00_00\\mmWaveStudio\\RunTime\\SAL.dll")
[12:21:18] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[12:21:18] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[12:21:18] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[12:21:18] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[12:21:18] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[12:21:18] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[12:21:18] RSTD.Transmit("/")
[12:21:18] RSTD.SaveSettings(): Settings saved to "C:\Users\Zber\AppData\Roaming\RSTD\config.xml"
[12:21:18] RSTD.Build()
[12:21:18] RSTD.SaveSettings(): Settings saved to "C:\Users\Zber\AppData\Roaming\RSTD\config.xml"
[12:21:18] RSTD.Transmit("/")
[12:21:18] RSTD.AL_Build()
[12:21:18] RSTD.AL_LoadXml()
[12:21:18] RSTD.Transmit("/")
[12:21:18] RSTD.AL_Init()
[12:21:18] RSTD.Clients_Build()
[12:21:18] GM: Init
[12:21:18] GM: Loaded 'C:\ti\mmwave_studio_02_01_00_00\mmWaveStudio\Clients\\LabClient.dll'
[12:21:18] GM: 1 Guest (s) init
[12:21:18] GM: 1 Module(s) init
[12:21:18] GM: 2 Tab (s) init
[12:21:18] RSTD.Client_LoadXml()
[12:21:18] [RadarAPI]: ar1.selectRadarMode(0)
[12:21:18] [RadarAPI]: Status: Passed
[12:21:18] Matlab Runtime Engine is installed
[12:21:18] [RadarAPI]: Starting Matlab Engine..
[12:21:20] [RadarAPI]: Matlab Engine Started!
[12:21:22] [RadarAPI]: ar1.selectCascadeMode(0)
[12:21:22] [RadarAPI]: Status: Passed
[12:21:22] [RadarAPI]: ar1.LoadSettings('C:\Users\Zber\AppData\Roaming\RSTD\ar1gui.ini')
[12:21:22] TESTING = false
[12:21:22] RstdNet: Port 2777: Listening..
[12:21:22]
[12:21:22] ***Script completed successfully.***
[12:21:24] [RadarAPI]: Opening Gpio Control Port()
[12:21:24] [RadarAPI]: Status: Passed
[12:21:25] [RadarAPI]: Opening Board Control Port()
[12:21:25] [RadarAPI]: Status: Passed
[12:21:26] [RadarAPI]: ar1.FullReset()
[12:21:26] [RadarAPI]: Status: Passed
[12:21:27] [RadarAPI]: Closing Board Control Port()
[12:21:27] [RadarAPI]: Status: Passed
[12:21:27] [RadarAPI]: Closing Gpio Control Port()
[12:21:27] [RadarAPI]: Status: Passed
[12:21:27] [RadarAPI]: ar1.SOPControl(2)
[12:21:27] [RadarAPI]: Status: Passed
[12:21:28] [RadarAPI]: ar1.Connect(3,115200,1000)
[12:21:29] [RadarAPI]: ar1.Calling_IsConnected()
[12:21:30] [RadarAPI]: ar1.SelectChipVersion("AR1642")
[12:21:30] [RadarAPI]: Status: Passed
[12:21:30] [RadarAPI]: ar1.SelectChipVersion("AR1642")
[12:21:30] [RadarAPI]: Status: Passed
[12:21:30] [RadarAPI]: ar1.deviceVariantSelection("XWR1843")
[12:21:30] [RadarAPI]: Status: Passed
[12:21:30] [RadarAPI]: ar1.frequencyBandSelection("77G")
[12:21:30] [RadarAPI]: ar1.SelectChipVersion("XWR1843")
[12:21:30] [RadarAPI]: Status: Passed
[12:21:30] Device Status : XWR1843/QM/SOP:2/ES:2
[12:21:30] [RadarAPI]: ar1.SaveSettings('C:\Users\Zber\AppData\Roaming\RSTD\ar1gui.ini')
[12:21:33] [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_02_01_00_00\\rf_eval_firmware\\radarss\\xwr18xx_radarss.bin")
[12:21:34] [RadarAPI]: Downloading BSS Patch RPRC Binary..
[12:21:41] [RadarAPI]: ar1.GetBSSFwVersion()
[12:21:41] [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17))
[12:21:42] [RadarAPI]: ar1.GetBSSPatchFwVersion()
[12:21:42] [RadarAPI]: BSSPatchFwVersion:(01.02.05.02 (30/04/19))
[12:21:42] [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_02_01_00_00\\rf_eval_firmware\\masterss\\xwr18xx_masterss.bin")
[12:21:43] [RadarAPI]: Downloading MSS RPRC Binary..
[12:21:54] [RadarAPI]: ar1.GetMSSFwVersion()
[12:21:54] [RadarAPI]: MSSFwVersion:(01.02.05.02 (16/07/19))
[12:22:28] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[12:22:28] Status: Failed, Error Type: RESP TIMEOUT
[12:22:32] MSS Power Up async event was not received!
1. all 6 ports can be seen in the device manager
2. I can see the packages Ethernet
There are my device snapshot and mmWave studio screenshot
Could u help me solve this problem?
Kind regards,
Xi