Part Number: DRV425
Hi, I am wondering how to fully evaluate the DRV425 for noise. There are some noise densities listed, e.g., 1.5nT/root Hz for the sensor and 170nV/root Hz for the output voltage. There are also charts. My goal is to understand what the noise output of the DRV425 will be with respect to the sensed input magnetic field so that I can predict what the SNR is. I plan to feed a precision A/D with the DRV425 and I want to make sure I don't over specify the A/D. If it matters any, this is for a low sample rate project (<60Hz) and I am looking to measure small (less than the earths) magnetic fields to as high a resolution as possible. Thanks.