Other Parts Discussed in Thread: TMP006
Hi,
We've got a PCB, which we've got mounted a TMP006. We've prototyped and tested and its all working really well, very happy with the results.
We then moved to a short production run and the TMP006s all failed. On investigation the problem is that as soon as we use a protective coating around the TMP006 it seems to kill it. Note that we had masked the top of the sensor and sprayed on the conformal coating in the normal way. The top sensing surface was clean and unmarked.
Since then we've done lots of experiments and whatever product we use to seal the TMP006 onto the board we either get crazy readings from the TMP006, or no output at all, its just "dead".
Under a microscope we can see that there is a square in the middle of the sensor, and we assume that this needs to be free from contamination, but we cannot find anything about the requirements for this.
The problem for our product is that the PCB is not sealed and is used externally, and hence we need to add on some protection from the moisture.
We read on the datasheets that you have to keep the underneath clear of flux, and we've done this. Before we add a coating around the ship it is functioning perfectly. We've tried some very viscous sealants around the chip and are certain that it's not going underneath - the sealants are just providing a deal from the sides of the IC down to the PCB.
Can you offer any explanation or advice on what we should do? At the moment the only option to us is to add a mechanical seal over the chip with a germanium window, but the germanium window is really expensive and would require a PCB redesign. In this case it would be far cheaper to use a different temperature measurement method.
Does the "mystery" square at the center of the underside of the IC need to be vented to the atmosphere for it to work?
Is this mystery square very sensitive to some particular out gassing from sealants etc?
I've been working with ICs for my whole career, never come across anything like it! Please help us!!!