Hi,When TMP300 reaches the set temperature, is OUT low or high,could you help check it,tks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,When TMP300 reaches the set temperature, is OUT low or high,could you help check it,tks!
Hi,
The output of the TMP300 is normally high and is pulled low when the temperature threshold is tripped. You can see this by observing the open-drain output, which uses a pull-up resistor, which pulls the OUT pin high when the chip is floating (when the switch is not tripped).
Thanks for the question!
Audrey