This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDEP-01012: Building image for mmWave Studio

Part Number: TIDEP-01012


Hi,

We are trying to build the image from the mmWave Studio.

Compiling Vision SDK 3.7 using tda2xx_cascade_linux_radar and RADAR_STUDIO=yes is successful but when trying to connect to it from mmWave Stdio using the Cascade_Configuration_MIMO.lua script fails.

We were able to use a precompiled SD card image with mmWave Studio using the same script but would like to have the flexibility to compile and modify it - which currently does not work.

Note that in the communication it appears that when the SD card communicates with mmWave Studio it reports VISION_SDK_03_07_01_00. It appears the latest version available on your website is Vision SDK 3.07.00.00 from June 2019.

How can we build the Vision SDK so it would work with mmWave Studio?

If a new Vision SDK is required, where can we download it?

Many thanks,

Rani