Part Number: IWR6843ISK
Other Parts Discussed in Thread: DCA1000EVM, MMWAVEICBOOST


I am currently using a DCA1000EVM+IWR6843ISK+MMWAVEICBOOST in mmWave Studio. The goal is to be able to capture data using hardware triggers from an external source.
Acoording to above two threads, the procedures I followed are:
1) Set the trigger select to Hardware Trigger and hit trigger frame
2) Feed the pulse to SYNC IN on pin 9 of J6 connector
I keep getting the message: [RadarAPI]: No of files Captured: 0, Total no of frames for each device : 8
What should I do?
I am sending four pictures as an attachment.
Thanks!
Ayaka