Dear All,
I have an application trying with an extremly large coil: 2 m x 1 m with 3 turn (later can be 4 turns) for vehicle detection.
Now having ~60 uH and 33 nF serial resistance 0.3 Ohm. Sometimes noise is too large and seems the IC is not
able to filter to my frequency effectively and detecting double or multiple times of the base frequency. (similar case in FAQ)
But here when I try to use the deglitch filter its not effective. Of course because of my low frequency that I set.
What do you propose in this situation?
Thanks in advance/
Developer