Tool/software:
512 Byte MTU Exchange is required. so, how this module will support?. where do configure that.
we are using TI SDK version “4_30_00_08”. and in that we using the simple_peripheral example.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
512 Byte MTU Exchange is required. so, how this module will support?. where do configure that.
we are using TI SDK version “4_30_00_08”. and in that we using the simple_peripheral example.
Hello, are you refering to SimpleLink CC2640R2 SDK 4.30.00.08?
Yes , that says 247 is max but other semiconductor is supporting 512 my customer is asking this as requirement. So we need to give the solution.
thanks
Hi Jayaprakash,
Please find the following link about the Maximum Transmission Unit (MTU) for the CC2640R2 SDK 4.30.00.08. There is also a section on Configuring for Larger MTU Values.
Regards
Ivan