This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS53355: About VREG

Part Number: TPS53355

Tool/software:

Hi,

<Question>

Could you tell me why the voltage of VREG becomes 4V?

Could you tell me why the voltage of VREG changes to 5V after a certain time, and why the voltage drop of VOUT occurs?

<Background>

For several hours after the power is turned on, the voltage of VREG becomes 4V.

After a few hours, VREG (2ch) changes to 5V and the voltage of VOUT (1ch) drops as shown in the attached waveform.

At this time, the device is not operated (there is almost no load fluctuation).

Best Regards,

Nishie

  •  

    Can you please share the schematic and operating conditions?  (Vin, Vout, Switching Frequency, Loading current) 

    What is the VDD voltage when this occurs?

    Is there anything connected to BP other than a high-quality dielectric, low ESR, low ESL ceramic bypass capacitor?

    If there is, what is connected?

    How is enable driven?  It is pulled up by VIN as soon as VIN rises, or is it delayed from VIN?

    The 4V BP voltage prior to the shutdown and restart of the output voltage appears unsteady, like the BP regulator is overloaded.  There appears to be an additional drop on BP, which is likely triggering the BP regulator's UVLO, causing a shutdown and restart of the IC when the BP regulator returns to regulation.

  • Hi Peter-san,

    Thank you for your support.

    Can you please share the schematic and operating conditions?  (Vin, Vout, Switching Frequency, Loading current) 

    Vin=12V, Vout=1.2V, Iout=max 20A, Fsw=500kHz. I will send you a circuit diagram by private message.

    What is the VDD voltage when this occurs?

    VDD=12V.

    Is there anything connected to BP other than a high-quality dielectric, low ESR, low ESL ceramic bypass capacitor?

    If there is, what is connected?

    Could you check the circuit diagram?

    How is enable driven?  It is pulled up by VIN as soon as VIN rises, or is it delayed from VIN?

    I measured the VIN and EN waveforms(1ch:VIN, 2ch:EN). Is there any problem with these waveforms?

    Best Regards,

    Nishie

  • Hi Nishie, The team is looking into this and will reply to you within a few days

    Best regards,

    Britton

  • Hi Nishie-san,

    Can you please share the customer schematic with me via email?

    What is the VREG5 capacitor part number being used? Also, is this at room temp or other ambient temp - please specify what temp it is. 

    Is it possible to share the VIN, VREG, SW, VOUT waveforms during normal operation and when the dip occurs?

    Also, how many units are exhibiting this issue? Are there good boards on which you can try the unit showing this issue?

    Thanks,
    Amod

  • Hi Amod-san,

    Thank you for your reply.

    I sent you an email. I would appreciate it if you could check it.

    Best Regards,

    Nishie

  • Hi Nishie-san,

    I responded to your email just now. Let us continue the discussion there.

    Thanks,
    Amod