This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5013: 0.1M in an LM5013 design using the calculator

Part Number: LM5013

Tool/software:

Using the Rev. B calculator. Min V is 6, Normal is 24, Max is 80, output voltage is 3.3V at 3.5Amps. It is listing the Ruv value as 0.1M. That's with a CAPITAL M, so MEGA? Why not just say 100k, as the resistor above it, RPGOOD, its stated value is 100k.

So are they following m=milli, M=MEGA? Why?