Tool/software:
We have developed our hardware using LMR36510. Pin voltage has been set for 1.24V . at min Input voltage using Resistor divider with referenced as negative output voltage.
We observed that Sometimes it works as per the requirement . operating was uncertain sometimes .
To cross check this funactionality we used pspice simulation of LMR36510 .
In the simulation this does not work for 1.24V as enable pin with referenced to negative output voltage.
Can you help us with the simulation model to validate our hardware design?
Also is that indicate the requirement of Level shift for enable pin . while using it as IBB .