This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS50601A-SP: Maximum lead temperature during soldering

Part Number: TPS50601A-SP


Tool/software:

What is the maximum lead temperature that can be reached during soldering, in datasheet it is given as "N / A for Pkg Type"

  • Hello Sureshkumar,

    Please reference document SLVAEU0 "Hermetic Package Reflow Profiles, Termination Finishes, and Lead Trim and Form " on ti.com.

    It states that, "The package body temperature must not exceed 260°C at any time or the hermetic seal of the package will be damaged"

    Thanks,

    Andy