This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC25660: UCC256601 : LO, HO Pulse is not getting generated

Part Number: UCC25660

Tool/software:

Design Specs

Input voltage = 320V DC
Output Voltage= 48V DC, 5A

UCC25660DDBR IC is used and UCC25660X excel calculator has been used. Schematic has been attached.llc design.pdf

Operation
I have applied input voltage of 320V DC. After that i checked, at VCC(Pin 12) 12V is coming on the IC. 5v is generated at 5VP (Pin 8).

But LO (Pin11) and HO (Pin 15) are not generating pulses.