This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM82810: TPSM82810SILR

Part Number: TPSM82810


Tool/software:

Can TPSM82810SILR be used as an alternative to EN6347QA in my design? TI part should be military standard  

  • Hello,

    thanks for reaching out in E2E.

    I think the TPSM82810 would be a suitable alternative to the EN6347QA. But the maximum recommend input voltage is lower for the TPSM82810 (6V instead of  6.6V of the EN6347QA).

    The TPSM82810 is only available in catalog standard. Also other alternative modules (with integrated inductor) are in catalog standard. The discrete version (without integrated inductor) of the TPSM82810 is the TPS62810 and it is available in Automotive (TPS62810-Q1), Extended Temperature (TPS62810M) and HiRel Enhanced Product (TPS62810-EP) grade.

    Best regards,

    Andreas.