Part Number: CD74HC4016
Hello,
We have used CD74HC4016PW for many years and it has worked fine, lately we have seen that the switches are not switching to an as low of a voltage as they used to. The switching voltage at pins 13, 5 and 6 has not changed.
We were able to track it down to lot numbers, for example parts with marking number D1J4 works and switches at the voltages that has always switched around 0.2V , but parts with marking numbers A37R do not switch at the typical voltage and require a much lower voltage to switch almost -0.1V.
Have there been any changes between the 2 lots? We might still be able to use the newer lots but I am trying to figure out a root cause.
Any help would be appreciated.
Thank you