Part Number: LMR38010-Q1
LMR38010FSQDDARQ1 Failure Observation
We observed failure (short circuit) of two LMR38010FSQDDARQ1 devices.
Initially, the EN pin was directly connected to the VIN pin, and the circuit operated without any issues.
Later, a Common Mode Choke (CMC) was added in the input line to improve EMI/EMC performance, and the EN pin was connected to the Ignition (IGN) input instead of the IN pin. Following this change, the LMR38010FSQDDARQ1 devices started failing and became short-circuited.
Subsequently, 47 k series resistor was added in the EN pin path, after which the circuit has been operating reliably without any failures.
Could you help identify the possible root cause of this failure?
According to the datasheet, the EN pin can withstand voltages greater than 80 V, whereas our system input voltage is only 24 V, our total load current is 60mA and DC-DC output is 13V (24V to 13V), 400KHZ SW freq