This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can E2E add other members in reply notifications are on state when I post new thread?

Hello,

When I make a new post, I want other members receive reply notification condition. Is there any setting for doing this?

So far I need to ask to the members to change the setting "reply notification are off" to on. It would be helpful to skip this process.

Best regards,

Toshihiro Watanabe

  • Former Member
    0 Former Member

    Hello,

    There is no setting to push replies to other users automatically. However, if you know a User's username you can reference it in a reply using the @ symbol and they will receive a notification of that reply. For example,  .  Type the @ symbol and start typing a username.  The system will automatically lookup the username and attempt to autocomplete it.

    Thanks

    Bill