Part Number: TMUX7209
Dear Team,
Do we have any suitable solution as below require?
Please check, and recommend have suitable analog switch 54V& 10mA current MAX (2:1 )as below, thanks!

Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Jimmy,
At this time we don't have a switch that will pass 54V - our current highest rated voltage multiplexer will pass up to 44V (single supply max with VDD = 44V). We do have parts that can handle the voltage but they will be in a fault protection state (open circuited or high Z) so it wont pass the signal.
If you have other questions please let me know!
Best,
Parker Dodson