Other Parts Discussed in Thread: TLV9002-Q1
Hi team,
I don't use S1A and S1B pins and plan to connect these pin directly to GND.
Since DA and DB are both connected to the OPAMP positive terminal without any capacitor connected, there should be no current flowing path to S1A, S1B external to the device.
In this case, Can I connect S1A, S1B pin directly to GND without current limiting resistor?
I think it should be OK, but would like to double confirm because there is a description below in the pin FMA document on TI.com.
"S1A short to GND failure : Corruption of signal passed onto the DA pin. If there is no limiting resistor in the switch path
device damage possible"
regards,