This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CBTLV3257: VIH and VIL specs consult

Part Number: SN74CBTLV3257


Hi Team,

Does the VIH and VIL requirements in below table only refer to the OE and S pins? Or including all input pins (such as A and B pins)? Thanks.

Best,

Stanley.

  • The A and B pins are analog I/Os and do not switch, so they do not have switching thresholds.

  • Hi Stanley,

    Clemens is correct - the A and B pins are analog I/O's and do not have VIL/VIH thresholds. Digital signals can still be passed through analog switches but the analog switch pathway itself is essentially just a small resistor between the two pins that are connected  with some parasitic capacitance to ground. 

    Only the digital pins on our analog switches require you to meet the listed thresholds (OE / S) 

    If you have any other questions please let me know!

    Best

    Parker Dodson