Hi Team,
My customer would like to know if TS3L501E supports RGMII switch function or not.
Please let me know, thanks!
Patty Chuang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
My customer would like to know if TS3L501E supports RGMII switch function or not.
Please let me know, thanks!
Patty Chuang
Hi Patty,
I see that you have clicked resolved - I am not sure if you no longer have this problem, but in case you do.
The TSL501E can handle any protocol that falls into the following categories:
Voltage supply - VDD = 3V to 3.6V
Max current through switch - Max = +/- 128mA
Signal levels - Device can pass signals 0V to VDD, and with no ESD diodes to VDD, overvoltage events within abs max will not cause back powering.
Bandwidth - each differential channel has a typical BW of 600MHz - with the 8 channels the device can support up to BASE1000-T - which is 1000Mbps. There are 4 differential data lanes - which means each data lane is appx. going to hold 250Mbps - which when converted to device bandwidth (multiply data rate by 1.5 - 3) and you can see that each lane will require between 375MHz and 750MHz of bandwidth - since this device usually has 600MHz of bandwidth per channel this part can support 1000Mbps.
To check if the bandwidth will work for your application follow the following formula:
1. Find total data rate
2. divide needed data rate by number of channels (for differential signals on the TSL501E this leaves us with 4 Lanes)
3. Multiply resulting data rate by 1.5x and 3x -> if the answer is in-between 1.5x and 3x data-rate there will be some minor attenuation, and above 3x there will be little to no attenuation due to frequency.
This device should be able to work in a lot of applications but it depends on exactly on how this is implemented.
If you have any questions please don't hesitate to reach out!
Best,
Parker Dodson