Hi,
I am currently using TMUX1072DGSR as the 2:1 MUX part. Do you have any 2:1 Mux part with the tristate option?
Regards.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Abhijith,
The TMUX1072 is an analog switch so there isn't defined outputs as you'd find in a digital multiplexer - most of TI's switches/multiplexers are analog so they they have a continuous band of outputs within the operating range and the switch can be open, closed, or high impedance -> but the switch itself is passive and doesn't drive anything.
That being said - I am adding in our Logic Product line because I believe they may have a few digital multiplexers that could potentially work- but it may be limited.
Best,
Parker Dodson