This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A3166: TS5A3166: unwanted input connects to output.

Part Number: TS5A3166

Hi There,

 In my application, 2.8VV battery voltage is always presence at Pin 1 and TS5A3166 5pinSOT-23 is powered from other system 3.3V rail. Below scenario i have seen:

NOTE: Pin 4 is pulled down to ground by 49.9K.

1) At power up/power down, observed the INPUT connects to OUTPUT (the battery voltage at input appears at the output) when system power transition between ~720mV to ~2.9V.

How do i fix this issue? Please advise.

Thanks,

Eric