This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX6219: What is the difference between Cs(OFF), Cd(OFF) and Cs(ON)/Cd(ON) in the datasheet

Part Number: TMUX6219

Hi,

Please let me ask you a basic question about "Capacitance" as below.

There are 3 specifications about it on the datasheet.

That is to say, 

  Cs(OFF) : 40pF(typ), Cd(OFF) : 58pF(typ), Cs(ON)/Cd(ON) : 150pF

Will you tell me the meaning of these capacitance?

Is this means between "each S, D pin" to "GND" in case "OFF"

and between "S" to "D" pin (parallelled ON registance) in case "ON"?

Thank you for your support.

Best Regards,

Takumi