Part Number: CD4066B
Other Parts Discussed in Thread: TS5A22364
I am using the CD4066 to choose one instrument (GUITAR IN Pin 1 / SITAR IN Pin 3) and output the selected one to a common output PEDAL IN (Pin 2). The appropriate LED would also light when selecting either input.
I am currently testing the circuit shown in the schematic below with the addition of 2.2MOhm resistors at GUITAR IN, SITAR IN and PEDAL IN. The circuit works fine, however I am getting a very audible Pop when switching the input. Does anyone know what can be done to reduce this pop?