This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1574: MUX between an High Speed differential-pair and 2 single-end LVCMOS clock

Part Number: TMUX1574


Hi TI Support Team,

I would like to use the TMUX1574 to multiplex a differential pair at 1.25Gbps with two single-end low frequency signals LVCMOS 1.8V  as indicated in the figure below:

The bandwidth is 2GHz however in typical applications there is the multiplexing between low frequency and single end signals such as SPI, JTAG, UART, I2C etc. Why?

Is the signal level compatible with both LVCMOS and LVDS ?

Thanks,

Massimiliano