Other Parts Discussed in Thread: TMUX1574, TS3A44159, TMUX1134, TMUX1575
Hi Team.
My customer has some issue of SN74CB3Q3257.
This is my customer specification,
I/O voltage is 1.8V
Vcc is 3.3V
Here is my customer question:
1.) According to this table. if Vcc is 3.3V, the VIH MIN voltage is 2V, does this mean if I/O voltage is 1.8V the output always low? If I want to avoid the problem, I need to reduce the VCC voltage?