PSPICE for TI could not open TMUX7212.dsn in scdm274.zip.
Could you give me a dsn file of the TMUX7212 PSPICE example in PSPICE for TI?
Regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
PSPICE for TI could not open TMUX7212.dsn in scdm274.zip.
Could you give me a dsn file of the TMUX7212 PSPICE example in PSPICE for TI?
Regards,
Hello,
I'm not seeing problems on my end opening up the file and have cross checked with a computer that didn't previously have PSPICE for TI installed yet so I don't think there is an issue with the file itself. Could you further explain what trouble you're seeing on your end?
Thanks,
rami
Hello rami-san,
Thank you for your quick response.
When I try to open TMUX7212.dsn, the PSpice outputs the following error:
ERROR(ORCAP-1653): Unable to load file.
'C:\work\PSPICE_TI\TMUX7212\tmux7212.dsn'
My PSpice for TI version is 17.4-2020 S004 SPB 640bit Edition.
Please let me know if the version you are using is different.
Thanks,
ikuo
Hello Ikuo-san,
Do the other files work fine? Could you try to run them in pspice without the dsn file? The dsn file provided is just an example circuit. Try following the instructions here https://training.ti.com/pspice-ti-3rd-party-model-import to get the model running in PSPICE for TI, going around the dsn file not opening issue.
I am running PSpice for TI version 17.4-2021 S007 SPB 64-bit Edition. I don't believe that should be an issue though.
You could try and install the latest version and it may resolve the issue but I can't guarantee this as a solution.
Thanks,
Rami