This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN74CB3Q3244: Some spec about SN74CB3Q3244

Part Number: SN74CB3Q3244

Hi team,

I want to ask two questions about using SN74CB3Q3244;

1. Does SN74CB3Q3244 support the transmission of VGA HSYNC (Horizontal Sync)/VSYNC (Vertical Sync) analog signals?
2. When Vcc is powered by 3.3V, can its IO input/output level be 5V?

Please help me check, thanks.