Other Parts Discussed in Thread: TMUX7208, TMUX6208
Hello everyone,
We are using the CD4051BPWR for multiplexing signals of +-3, +-6 and +-9 V, we've checked this values arrive to their respective pins.
The supply voltages are: VCC = 10V, VEE = -10V and VSS = 0V.
The control signals (A,B,C) are controlled by an ESP32 so their HIGH value is 3.3V, they also change correctly when it's necessary.
The enable pin is connected with a pull down resistor of 10K ohms.
However, we don't see any voltage in the output pin of the device.
I'm attaching a pic of the schematic.
Would appreciate any help or advice,
Thank you so much.