This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1072: Land pattern & solder paste example

Part Number: TMUX1072


Dear team, 

Can you help with land pattern & solder paste example for TMUX1072RUTR (UQNF-package)? 

Couldn't find it in the data sheet or on package /pins link on ti.com

Many thanks

Jorgen

  • Hi Jorgen,

    The Package Drawing is here: https://www.ti.com/lit/ml/mpqf248b/mpqf248b.pdf?ts=1642794611170&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FTMUX1072

    For some reason - this drawing does not include an example land - pattern and solder mask details - however other similar UQFN's do - and the rules that they have can be transcribed to the above drawing.

    The examples are a 10 pin UQFN and a 16 pin UQFN. 

    10 Pin: https://www.ti.com/lit/ml/mpqf206c/mpqf206c.pdf?ts=1642794856943&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FTMUX154E

    16 Pin: https://www.ti.com/lit/ml/mpqf205f/mpqf205f.pdf?ts=1642794759615&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FTMUX1113

    Using the 16 pin as an example - take a look at the package drawing , land pattern/solder mask (pattern and mask are same dimensions - please follow solder mask details on the 16pin or 10pin UQFN as it will be the same for the 12 pin as with the 1072) (shown below):

    Package Drawing:

    Variables: 

    L = Length = Typical 1.8mm

    W = Width = Typical 2.6mm

    TP =  Top and Bottom Oriented Pins Length = Typical 0.4mm

    SP = Side Oriented Pins Length = Typical 0.5mm

    PW = Pin Width = 0.2mm

    E = Pitch = 0.4mm

    -----------------------------------------------------------------------------------------------------------------------------

    Land Pattern Drawing:

    Variables:

    L_LP = Length of Land Pattern = 1.6mm

    W_LP = Width of Land Pattern = 2.4mm

    TP_LP =  Top and Bottom Oriented Pins Length of Land Pattern= 0.6mm

    SP_LP = Side Oriented Pins Length of Land Pattern = 0.7mm

    PW_LP = Pin Width of Land Pattern = 0.2mm

    E_LP = Pitch of Land Pattern = 0.4mm

    If you look at how these dimensions change - its actually standardized between pin counts (look at the 10 pin package and the same pattern will emerge) - which is the following:

    L_LP = Length of Land Pattern = L - 0.2mm

    W_LP = Width of Land Pattern =W - 0.2mm

    TP_LP =  Top and Bottom Oriented Pins Length of Land Pattern= TP + 0.2mm

    SP_LP = Side Oriented Pins Length of Land Pattern =SP + 0.2mm

    PW_LP = Pin Width of Land Pattern = PW

    E_LP = Pitch of Land Pattern = E

    TMUX1072 Land Pattern Dimensions

    Which when we plug that in for the TMUX1072's UQFN package we get the following results:

    L = Length = Typical 2mm

    W = Width = Typical 1.7mm

    TP =  Top and Bottom Oriented Pins Length = Typical 0.5mm

    SP = Side Oriented Pins Length = Typical 0.4mm

    PW = Pin Width = 0.2mm

    E = Pitch = 0.4mm

    Converting that into the Land Pattern Measurements:

    L_LP = Length of Land Pattern = L - 0.2mm = 1.8mm

    W_LP = Width of Land Pattern =W - 0.2mm = 1.5mm

    TP_LP =  Top and Bottom Oriented Pins Length of Land Pattern= TP + 0.2mm = 0.7mm

    SP_LP = Side Oriented Pins Length of Land Pattern =SP + 0.2mm = 0.6mm

    PW_LP = Pin Width of Land Pattern = PW = 0.2mm

    E_LP = Pitch of Land Pattern = E = 0.4mm

    For the Solder Mask Please see below:

    This is the same details we recommend on all our UQFN switches.

    If you have any other questions please let me know!

    Best,

    Parker Dodson

  • Hi TI team,

    Thank you for this post information! 

    Would be possible to get an official land pattern drawing for TMUX1072? It would be needed for usage and storage in our database.

    Thank you!

    Best,

    Cora Ferrer

  • Hi Cora,

    Please see the link here - https://app.ultralibrarian.com/details/16967dbf-103f-11e9-ab3a-0a3560a4cccc/Texas-Instruments/TMUX1072RUTR?uid=94115702 

    That is our footprint file. 

    We are working on adding the official drawing to the datasheet - but this may take a while as we have a few processes and multiple people to go through  to add new package drawings. 

    If you have any other questions please let me know!

    Best,

    Parker Dodson