The project is to monitor large Fuel cell pack voltage.
My customer have 24 fuel cells in series, so the overall pack voltage is 9-26.5V.
Still now they used LTC6808, which is a great chip, but as get in shortage they need a less chip dependent design.
Im thinking to use a TMUX6211/DG412 as input MUX as that is available at several manufacturers. This muxes (12 pcs) would select 1 by 1 the cells, and connect them to an ADC. Vs are inputs, while Vd are outputs to ADC.
Here I have already a question about powering the mux. Can I power them directly from the cells 9-26.5V ? Will they work fine close to the rails (VDD=Vs) ? Based on datasheet they can work, but as I need to measure at 10mV level, I need really full rail to rail working range for the switched signals.
The cells can go slightly on negative too, so if the pack GND is used as GND for the muxes (connected to VSS), than it can happen as cell 1 goes negative, so the switch input Vs pin have for ex. -1V less than its main GND (GND and VSS).To avoid this actually I added 2 DC-DCs. One to boost the pack voltage (9-26.5V) to fixed 30V to power the VDD of the muxes, and other one like -3V to power the VSS as GND of the muxes used as GND of the system.
Based on datasheet "Source or drain voltage (Sx, Dx) VSS–0.5 VDD+0.5" so mainly should work well for inputs on + side (Vs=VDD) and down to -0.5V on negative side(Vs=VSS-0.5V), but we dont want to lose any mV due clamping or any internal protection.
Could anyone tell me if im on the right way and really both DC-DC are needed ?
OR
Thank You !
Zoltan