This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TS5A23160: Peak ON Resistance with 1.8V Supply

Part Number: TS5A23160
Other Parts Discussed in Thread: TS5A23159, TS3A24159

Hello,

I see the Peak ON Resistance across temperature for this device with 1.8V supply is 30 Ohms. Is this correct? For other supply voltages this ranges between 1.1 - 2.7 Ohms.

Thanks,

Michael

  • Hey Michael,

    I would trust the datasheet value on this. On the lower supply voltage you'll sometimes see some performance degradation in some devices. Take a look at the TS5A23159, which is mostly a logic variant of the 23160. The peak is 15ohms.
    What's the application here? Is the On-capacitance a concern. If that on resistance is still too high for your application and capacitance isn't a huge concern, the TS3A24159 has a small supply range so it performs better with a 1.8V supply. The peak here is just 0.8ohms across temperature. Caveat is an increase in On capacitance.

    Thanks,
    Rami

  • Thanks Rami! We actually started with TS3A24159 but moved to TS5A23159 because of available inventory.