Other Parts Discussed in Thread: TMUX1104
Hello,
My customer use only channel A.
In this case, can they leave S1B, S2B, S3B, S4B and DB floating?
If not, please let them know recommended terminations for those pins.
Best regards,
K.Hirano
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Kazuhiko,
If only one channel is being used, you can leave the signal pins floating. In higher speed applications it's good practice to terminate these to ground through a 50ohm resistor, however.
See TI Precision Labs - Can I leave unused pins floating?
What voltages are they using? If it's between 1.08 and 5.5V (they aren't using dual supply) the TMUX1104 is a 4:1 1 channel that may be a good replacement if they aren't using the second channel of the TMUX1109.
Thanks,
Rami