Hi,
My customer is wondering if he can get 1.8V on the A1,A2,B1,B2 pins when Vcc = 0V and an external chip is driving the data lines A1,A2 or B1,B2?
Does this snip below from the DS answer this question?
Thanks and best regards,
Johan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
My customer is wondering if he can get 1.8V on the A1,A2,B1,B2 pins when Vcc = 0V and an external chip is driving the data lines A1,A2 or B1,B2?
Does this snip below from the DS answer this question?
Thanks and best regards,
Johan
Hi Johan,
You are correct. The absolute max condition for input/output DC voltage is not dependent on the supply voltage VCC. Therefore, when VCC = 0V, your I/O pins can be between -0.3V and 5.5V. I would go off of the recommended operating conditions instead so that you do not accidently push the device over its abs. max ratings.
Another way to see if this is okay is to check the power-off leakage current (IOFF) spec. This is the same test setup as shown in Figure 7-3 of the datasheet for the IOZ spec, except VCC = 0V.
When VCC = 0V and voltage on A1/A2 is ramped from 0V to 3.6V, we see a small amount of leakage appear on the COM pin, telling us there is separation between I/O pins.
Also, this FAQ is a helpful resource for answering the most commonly asked questions about our switches and multiplexers portfolio.
Regards,
Tyler