This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMUX1111: Leakage Current

Part Number: TMUX1111

Hi,

I'm using the switch TMUX1111PWR in a QVAR measure application.

I need a switch with a very low leakage current that not affect the measure and my choice was the TMUX1111PWR.

The datasheet shows a leakage current ID(OFF) about 1pA min or 50pA max at VDD=3.3V and 25°C. Is correct?

On real application I'm seeing a Leakage current IDOFF (on Drain when switch is open) higher than the max expected, also till 100pA. 

Can you suggest a way to reduce this current at 10pA?

Thanks

Corrado