I was using PSpice model of TMUX1101 in TINA to simulate the functionality of this switch. As per what I understand from datasheet, TMUX1101 is turn on when SEL is 1 and turn off then SEL is 0.
However, when I input 0V to SEL, i still can see voltage passing through from S to D. Is this the TMUX1101 suppose to be?