Other Parts Discussed in Thread: TMUX1248
Hi Sir:
I have a application which needs switch 8MHz and 24 MHz clock signal. Does SN74LCV3157 meet this application ??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir:
I have a application which needs switch 8MHz and 24 MHz clock signal. Does SN74LCV3157 meet this application ??
Hey Jim,
Yes, the SN74LVC3157 will meet your bandwidth requirements as long as the voltage is between 0 and 5V.
I would also recommend you to take a look at the TMUX1248 which is a higher performing new product. This is a drop-in match to the SN74LVC3157 with lower on resistance and logic compatible from 1.8 to 5.5V. It will include extra features such as fail-safe logic. See TI precision lab video : What is fail-safe logic?
Thanks,
Rami