Hi Team,
I don't see much detail in the datasheet. My customer is trying to run the device at 5V and potentially have some 5V inputs as well. From what I understand the outputs can only go up to VCC-1 so the output with 5V input will be 4V. However, I want to know if there are any other concerns with having the input levels and VCC be the same other than the output attenuation (damage, wrong operation, etc). Thanks!
Cheers,
Fadi